:SPRocess:RRX:PNOise:BANDwidth
Command Syntax
:SPRocessN:RRX:PNOise:BANDwidth <bandwidth>
Where <bandwidth> is the bandwidth. For example, 1.2e9.
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:RRX:PNOise:BANDwidth?
Description
Sets the bandwidth used when preserving the input waveform's noise on the output waveform. To turn on noise preservation, use the :SPRocess:RRX:PNOise parent command. The :SPRocess:RRX:PNOise:BANDwidth:AUTO command must be set to OFF otherwise the function automatically determines the bandwidth to use.
What function do I address this command to?
Always address the :SPRocess:RRX:PNOise:BANDwidth command to the Reference Rx's output function. In the following figure of the Reference Rx Setup dialog's operator diagram, this would be Function 2. In this case, the command would be:
:SPRocess2:RRX:PNOise:BANDwidth 1.5e9
Requires FlexDCA revision A.07.80 and above.