:SPRocess:RRX:PRESets:SELections?
Query Syntax
:SPRocessN:RRX:PRESets:SELections?
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Response
"Setting-A,Settings-B,..."
Description
For the Reference Rx operator, returns the a list of presets that have been saved for the operator. These presets include all of the setting for this operator including the settings for the CTLE, Linear Equalizers, and Non-Linear Equalizer.
What function do I address this command to?
Always address the :SPRocess:RRX:PRESets:SELections? command to the Reference Rx's output function. In the following figure of the Reference Rx Setup dialog's operator diagram, this would be Function 2. In this case, the command would be:
:SPRocess2:RRX:PRESets:SELections?
TDECQ Equalizer Presets
- IEEE 802.3dj Draft 2.0
- IEEE 802.3bs Amended
- IEEE 802.3bs
- IEEE 802.3cd
- IEEE 802.3db SR SECQ
- IEEE 802.3db SR (844-863 nm)
- IEEE 802.3db VR (842-948 nm)
- IEEE 802.3db VR (842-918 nm)
- IEEE 802.3db VR (842-888 nm)
- IEEE 802.3db VR (842-868 nm)
- Fiber Channel PI - 7 Rev 0.13
- TDEC ITU 50G PON OLT
- TDEC ITU 50G PON ONU
Requires FlexDCA revision A.07.80 and above.