:SYSTem:FACTory
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Command Syntax
:SYSTem:FACTory
Description
Sets FlexDCA to its factory preset settings. Use the *OPC? query to notify the calling program when an operation is complete. Factory preset is the combination of the default settings and additional settings. There is no query form of this command or ability to undo its action.
Use of an *OPC? query to pause program execution while waiting for this command to execute.
| Feature | Setting |
|---|---|
| Miscellaneous Settings | |
| List of recent setup files | Cleared |
| List of recent DCA-X hosts | Cleared |
| Use Compact Signals Palette | Off |
| Show Marker Tools on Screen | On |
| Multi-Purpose button | Removes any configuration settings |
| Display Setup dialog Settings (Appearance Tab) | |
| UI Theme | Tungsten |
| Show Animations | on |
| Dialog Size | Normal |
| Mode Switch Animation | No Animation |
| Overlap Display Tabs | off |
| Use On-Screen Keyboard | off |
| Connection Setup Dialog Settings | |
| On Connect Setting | Restore |
| Connection Type to DCA-X | LAN |
| SICL Interface | gpib0 |
| GPIB Address | 7 |
| SCPI Server Setup | |
| GPIB | Enabled |
| VXI-11 | Enabled |
| USB | Enabled |
| Telnet | Disabled |
| Sockets | Enabled |
| USB | Enabled |