:SYSTem:LAUNch
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Command Syntax
:SYSTem:LAUNch <string>
<string> is the name of an installed DCA-X compliance application.
Description
Launches a DCA-X compliance application, such as the N1012A OIF CEI 3.0 application. Installed applicatons appear on the Apps > Automated Test Apps menu. To determine the proper string, perform the following steps:
- Click Tools > SCPI Programming Tools > SCPI Recorder to turn on the SCPI recorder.
- Click the Record button.
- Click Apps > Automated Test Apps following by the application that you want to launch.
- The recorder shows the :LAUNch command with the correct string.
Requires FlexDCA revision A.02.00 and above.
Example Command Sequence
:SYSTem:LAUNch "N1012A OIF CEI 3_0"