:SYSTem:VIEW
Command Syntax
:SYSTem:VIEW {CHAN{N} | DIFF{1:8}{A|C} | CMOD{1:8}{A|D} |
FUNCtion{1:64} | WMEMory{1:8} | TRACe{1:128} | JMEMory1 |
CGMemory{1:8} | HISTogram{1:4}}
Where CHANnel{1:8}{A:D} is a channel. For example, CHANnel2B.
Where DIFF{1:8}{A|C} is a differential channel. For example, DIFF4C.
Where CMOD{1:8}{A|C} is a common-mode channel. For example, CMOD2C.
Where FUNCtion{1:64} is a math function. For example, FUNCtion8.
Where WMEMemory{1:8} is a waveform memory. For example, WMEMory2.
Where TRACe{1:128} is a trace. For example, TRACe5.
Where JMEMory1 is the jitter memory. For example, JMEMory1.
Where CGMemory{1:8} is a color-grade memory (eye diagram). For example, CGMemory2.
Where HISTogram{1:4} is a histogram. For example, HISTogram3.
Description
Turns on an active channel, differential waveform, common-mode waveform, function, waveform memory, color grade memory, jitter data memory, or histogram. Use the SYSTem:BLANk command to turn them off.
The JMEMory1 argument is only valid when FlexDCA is in Jitter Mode. If FlexDCA is not in Jitter Mode, this argument does not place FlexDCA in Jitter Mode. The JMEMory1 waveform can be viewed in Jitter Mode's Waveform panel.
When FlexDCA is in Jitter Mode, send a :SYSTem:AUToscale command to properly scale the waveform.
The Interactive SCPI Command Tree lists additional ACHannel0A and ACHannel0B arguments for this command. These arguments are reserved for internal Keysight use and have no effect when used by a customer.