:SYSTem:STAutodetect
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SYSTem:STAutodetect
Description
Detects the signal type for all of the following displayed waveforms: channels, common-mode channels, differential channels, and functions. Signals can be detected as clock, NRZ, or PAM4. Automatic signal-type detection is enabled by default, but you can disable it for any particular waveform using one of the following commands:
Signal-type detection is also run as part of an autoscale (:SYSTem:AUToscale).
Use of an *OPC? query to pause program execution while waiting for this command to execute.
Requires FlexDCA revision A.04.50 and above.
Example Command Sequence
:CHANnel2A:SIGNal:TYPE:AUTO ON :SYSTem:STAutodetect;*OPC? :CHANnel2A:SIGNal:TYPE?