:SYSTem:FUNCtions:OFF
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SYSTem:FUNCtions:OFF
Description
Deletes all created Waveform Signal Processing functions from the Waveform Signal Processing Setup dialog's Operators palette. In addition, any defined function output waveforms are turned off. This removes all waveform signal processing.
While there is no SCPI command to restore your function definitions, you can undo this action by clicking Setup > Undo from FlexDCA's front panel. Or, you can recreate your functions using the commands in the :FUNCtion and :SPRocesssubsystems.
Requires FlexDCA revision A.06.81 and above.