:SYSTem:GTLocal
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Command Syntax
:SYSTem:GTLocal
Description
Places FlexDCA in local mode which allows operation via the front panel. This is useful if you need the user to perform a front-panel task. The next command that is sent to the instrument returns it to remote mode. When ending a program, you should always issue this command to return control to the front panel.
Requires FlexDCA revision A.02.00 and above.