:TIMebase:DESKew:CSIGnaling:CANCel
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
:TIMebase:DESKew:CSIGnaling:CANCel
Description
Cancels a CNRZ5 Deskew procedure (:DESKew:CSIGnaling command) that is in process. The :CANCel command is equivalent to clicking a procedural dialog's Cancel button. Use the :DESKew:CSIGnaling:CONTinue command to start the next segment of the procedure. Use the :DESKew:CSIGnaling:SDONe command to wait and test for the successful completion of a procedural step.
Requires FlexDCA revision A.06.40 and above.