:TIMebase:DESKew:CSIGnaling:FUNCtion
Command Syntax
:TIMebase:DESKew:CSIGnaling:FUNCtion FUNCtionN
Where N identifies one of sixty four {1:64} math functions that you can create. For example, FUNCtion2.
Query Syntax
:TIMebase:DESKew:CSIGnaling:FUNCtion?
Description
When two or more CNRZ5 Decode operators are displayed, send this command to select the CNRZ5 Decode operator for which you want to deskew the input waveforms. The operator is selected by indicating one of the operator's output functions. For example, the following figure shows two CNRZ5 operators. If you wanted to deskew the top operator's input waveforms, you would send the command with any of the following arguments: FUNCtion1, FUNCtion2, FUNCtion3, FUNCtion4, or FUNCtion5. To select the bottom operator, use any of the following arguments: FUNCtion6, FUNCtion7, FUNCtion8, FUNCtion9, or FUNCtion10.
If only one CNRZ5 Decode operator is displayed, FlexDCA automatically sets the correct function. The query form of the command returns the selected function.
Requires FlexDCA revision A.06.40 and above.