:TIMebase:DESKew:CSIGnaling:SDONe?
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Query Syntax
:TIMebase:DESKew:CSIGnaling:SDONe?
Query Response
unknown
Description
Waits for the completion of a CNRZ5 operator deskew step and returns either an error message or a message that indicates success (a decision dialog is displayed). Use the :DESKew:CSIGnaling:CONTinue to begin the next step or the :DESKew:CSIGnaling:CANCel command to abort the procedure.
If the CNRZ5 Deskew has not been initiated, the following string is returned:
"No fixture deskew in progress."
Requires FlexDCA revision A.06.40 and above.