:TIMebase:DESKew:CSIGnaling:SAVE
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
:TIMebase:DESKew:CSIGnaling:SAVE {ON | OFF | 1 | 0}
Query Syntax
:TIMebase:DESKew:CSIGnaling:SAVE?
Query Response
{ON | OFF | 1 | 0}
Description
Enables or disables the saving of the CNRZ5 operator's deskew generated skew results data to an instrument setup file. When enabled, the data is saved with the setup files specified with the :DESKew:CSIGnaling:FNAMe command.
Requires FlexDCA revision A.06.40 and above.