:TIMebase:DESKew:CSIGnaling
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
:TIMebase:DESKew:CSIGnaling
Description
Deskews the input signals on a CNRZ5 custom waveform signal processing operator (:FUNCtion:FOPerator CNRZ5). The deskew, for each channel, includes the full function chain leading up to the operator. Deskew works with channel inputs but not waveform memory inputs. For optimal speed and accuracy, configure the DUT for a short PRBS pattern before running deskew. A PRBS-9 pattern is recommended. When two or more CNRZ5 Decode operators are displayed, send the :DESKew:CSIGnaling:FUNCtion child command to select the CNRZ5 Decode operator for which you want to deskew the input waveforms.
Requires FlexDCA revision A.06.40 and above.