:TIMebase:DESKew:FIXTure:CANCel
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
:TIMebase:DESKew:FIXTure:CANCel
Description
Cancels a Fixture Deskew procedure (:DESKew:FIXTure command) that is in process. The :CANCel command is equivalent to clicking a procedural dialog's Cancel button. Use the :DESKew:FIXTure:CONTinue command to start the next segment of the procedure. Use the :DESKew:FIXTure:SDONe command to wait and test for the successful completion of a procedural step.
Requires FlexDCA revision A.02.00 and above.
Example Command Sequence
Refer to the :DESKew:FIXTure command for a complete example.