:TIMebase:DESKew:CSIGnaling:CONTinue
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
:TIMebase:DESKew:CSIGnaling:CONTinue
Description
Continues a CNRZ5 Deskew procedure (:DESKew:CSIGnaling command) that is in process. The :CONTinue command is equivalent to clicking a procedural dialog's Next button. Use the :DESKew:CSIGnaling:CANCel command to abort the procedure instead. Use the :DESKew:CSIGnaling:SDONe command to wait and test the succsessful completion of a procedural step.
Requires FlexDCA revision A.06.40 and above.