:TIMebase:DESKew:FIXTure:SDONe?
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Query Syntax
:TIMebase:DESKew:FIXTure:SDONe?
Query Response
Returns a string.
Description
Waits for the completion of a Fixture Deskew step and returns either an error message or a message that indicates success (a decision dialog is displayed). Use the :DESKew:FIXTure:CONTinue to begin the next step or the :DESKew:FIXTure::CANCel command to abort the procedure.
If the Fixture Deskew has not been initiated, the following string is returned:
"No fixture deskew in progress."
Requires FlexDCA revision A.02.00 and above.
Example Command Sequence
Refer to the :DESKew:FIXTure command for a complete example.