:TIMebase:DESKew:FIXTure:SAVe
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
:TIMebase:DESKew:FIXTure:SAVe {ON | OFF}
Query Syntax
:TIMebase:DESKew:FIXTure:SAVe?
Description
Enables or disables the saving of the fixture deskew generated skew results data to an instrument setup file. When enabled, the data is saved with the setup files specified with the :DESKew:FIXTure:FNAMe command.
Requires FlexDCA revision A.02.00 and above.
Example Command Sequence
Refer to the :DESKew:FIXTure command for a complete example.