:TRIGger:CRATe
Instrument
N1000A
N109X
Flex Apps:
FlexDCA
Command Syntax
:TRIGger:CRATe <rate>
<rate> is a double.
Query Syntax
:TRIGger:CRATe?
Description
When a Fractional clock ratio for pattern lock is selected using the :TRIGger:DCDRatio:TYPE command, use the :TRIGger:CRATe command to enter the actual clock rate. For example, for an 9.95328 GBd input signal you could enter:
:TRIGger:CRATe 4.97664E9
Requires FlexDCA revision A.06.80 and above.
Example Command Sequence
:TRIGger:DCDRatio:TYPE FRACtional :TRIGger:CRATe 4.97664E9