:TRIGger:DCDRatio:TYPE
Instrument
N1000A
N109X
Flex Apps:
FlexDCA
Command Syntax
:TRIGger:DCDRatio:TYPE {INTeger | FRACtional}
Query Syntax
:TRIGger:DCDRatio:TYPE?
Description
Enters the clock ratio for pattern lock. Select either an integer sub rate of the symbol rate (INTeger) or a fraction sub rate of the symbol rate (FRACtional).
INTeger- Enter an integer clock divide ratio using the
:TRIGger:DCDRatiocommand. To apply the ratio, disable autodetection (:TRIGger:DCDRatio:AUTodetect). In some situations, you may need to enter a trigger divide ratio for a trigger that is a divided rate from the data rate. For example, for rates greater then 23.2 Gbs, you must provide a divided trigger. When this setting is selected, the following commands are available::TRIGger:SRATe:AUTodetect(Symbol Rate):TRIGger:DCDRatio:AUTodetect(Clock Divide Ratio):TRIGger:PLENgth:AUTodetect(Pattern Length):MEASure:JITTer:DEFine:SIGNal:AUTodetect(Signal Type for Jitter Mode)
FRACtional- Enter an fractional clock rate using the
:TRIGger:CRATecommand. Autodetection is not applied so the commands listed above for Integer clock ratios have no effect.
Requires FlexDCA revision A.06.80 and above.