:TRIGger:DCDRatio:FRACtion
Instrument
N1000A
N109X
Flex Apps:
FlexDCA
Query Syntax
:TRIGger:DCDRatio:FRACtion?
Query Response
Returns a float. For example, 1.60E+10.
Description
Returns the fractional clock ratio when a fractional clock is selected with the :TRIGger:DCDRatio:TYPE command.
Requires FlexDCA revision A.06.80 and above.