:TRIGger:MRATe?
Instrument
N1000A
N109X
Flex Apps:
FlexDCA
Query Syntax
:TRIGger:MRATe?
Description
For the N1000A DCA-X and DCA-M oscilloscope modules, returns the measured clock rate at the Clock In input of the oscilloscope. The query requires that the following be true:
- At least one of the channel's must be on (although the channel input data does not need to be connected).
- There has been at least one data acquisition. (
:ACQuire:RUNor:ACQuire:SINGle)
This command does not apply to FlexRT mode for UXR oscilloscopes, or the FlexEye Independent Eye Acquisition streaming feature.
Requires FlexDCA revision A.05.70 and above.