:TRIGger:DCDRatio:AUTodetect
Instrument
N1000A
N109X
Flex Apps:
FlexDCA
Command Syntax
:TRIGger:DCDRatio:AUTodetect {ON | OFF | 1 | 0}
Query Syntax
:TRIGger:DCDRatio:AUTodetect?
Query Response
{1 | 0}
Description
Enables or disables automatic detection of trigger-divide-ratio for pattern lock. A default setup turns automatic detection on.
When automatic detection is turned off, use the :TRIGger:DCDRatio command to enter the ratio. When automatic is enabled, send the :TRIGger:PLOCk ON or :SYSTem:PAUTodetect command to actually detect the trigger-divide-ratio.
This command requires that the type of Clock Ratio be first set to Integer instead of Fractional. Use the :SLOT:DCDRatio:TYPE command to select an integer clock ratio.
This command applies to an N1092A/B/D Option-PLK DCA-M.
Example Command Sequence
:TRIGger:DCDRatio:TYPE INTeger :TRIGger:DCDRatio:AUTodetect OFF :TRIGger:DCDRatio SUB4