:TRIGger:PLENgth:AUTodetect
Instrument
N1000A-PLK
N1092x-PLK
N1093A/B-PLK
N1094A/B-PLK
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:TRIGger:PLENgth:AUTodetect {ON | OFF | 1 | 0}
Query Syntax
:TRIGger:PLENgth:AUTodetect?
Query Response
{1 | 0}
Description
Enables or disables automatic detection of pattern-length for pattern lock. A default setup turns automatic detection on.
When automatic detection is turned off, use the :TRIGger:PLENgth command to enter the pattern length. When automatic is enabled, send the :TRIGger:PLOCk ONor :SYSTem:PAUTodetect command to actually detect the pattern length.
This command requires that the type of Clock Ratio be first set to Integer instead of Fractional. Use the :TRIGger:DCDRatio:TYPE command to select an integer clock ratio.
This command applies to an N1092A/B/D Option-PLK DCA-M.
Example Command
:TRIGger:DCDRatio:TYPE INTeger :TRIGger:PLENgth:AUTodetect ON