:CALibrate:OPTical:UCURrent
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Command Syntax
:CALibrate:OPTical:UCURrent
Query Syntax
:CALibrate:OPTical:UCURrent?
Description
During a Hardware Diagram paths calibration, forces the calibration to use an optical path's measured attenuation if that attenuation is above the maximum allowed value set with the
command.:CALibration:OPTical:MATTenuation