:CALibrate:OPTical:LOAD:FNAMe
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations
Command Syntax
:CALibrate:OPTical:LOAD:FNAMe
Query Syntax
:CALibrate:OPTical:LOAD:FNAMe?
Description
Specifies a custom calibration file name (including path and extension) for:
- Importing an optical calibration file into FlexOTO memory using the
:CALibrate:OPTical:LOAD) command. - Saving an optical calibration to a file.
- Saving a partial optical calibration to a file using the
:CALibrate:OPTical:SPARtial) command.
If you do not send this command, FlexOTO will automatically generate a name, which can be queried sending :CALibrate:OPTical:LOAD:FNAMe?. This command is equivalent to clicking Browse in the Optical Calibration dialog.