:CALibrate:OPTical:STEP:COUNt?
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations
Query Syntax
:CALibrate:OPTical:STEP:COUNt?
Description
Returns the total number of steps in the current Optical Calibration. This is the number of steps that calibrate an optical path (Fixture / Lane input to switch output). This count does not include starting and ending calibration steps. To return the step number for current calibration step, use the :CALibrate:OPTical:STEP query.