:CALibrate:OPTical:LOAD
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Command Syntax
:CALibrate:OPTical:LOAD
Query Syntax
:CALibrate:OPTical:LOAD?
Description
Loads an optical calibration file (*.ocdx) into FlexOTO memory. If no file name is specified using the :CALibrate:OPTical:LOAD:FNAMe) command the name of the last file created will be used. The loaded calibration must match the current hardware diagram's:
- DCA-M module model numbers,
- DCA-M serial numbers, and
- Existing paths.
Use the :CALibrate:OPTical:STATus? query to determine if the loaded calibration is valid or invalid and, if invalid, the :CALibrate:OPTical:STATus:REASon? query to determine the reason. For example, "Missing module". From the GUI, a warning is displayed and you can click Details in the Calibrations dialog.