:CALibrate:OPTical:STATus?
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Command Syntax
:CALibrate:OPTical:STATus
Query Syntax
:CALibrate:OPTical:STATus?
Query Response
{CORR | INValid | VALid}
Description
Queries the status of the optical calibration. If the returned string is not "CORR", use the :CALibrate:OPTical:STATus:REASon? query to determine the reason for a invalid or questionable measurement. If the measured optical loss through a path is greater than allowed by the :CALibrate:OPTical:MATTenuation command, the status of the optical calibration will be set to INValid.