:CALibrate:OPTical:CONTinue
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations
Command Syntax
:CALibrate:OPTical:CONTinue
Description
Continues all optical path calibrations that are in process. As a calibration progresses, message or decision dialogs often appear. For example, the user might be instructed to disconnect any front-panel inputs to a module. This command is equivalent to clicking the dialog's Next or Done button. Use the CALibrate:OPTical:CANCel command for an equivalent of the Cancel button.
Follow this command with the query to control program timing.:CALibrate:OPTical:SDONe?