:CALibrate:OPTical:ENABle
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Command Syntax
:CALibrate:OPTical:ENABle [ON | OFF]
Query Syntax
:CALibrate:OPTical:ENABle?
Description
Enables or disables an optical calibration of all of the optical paths in the Hardware Diagram. To create an optical calibration, use one of the following methods:
- Start and create a calibration with the
:CALibrate:OPTical:STARtcommand. - Load a previously saved calibration file into FlexOTO memory using the
:CALibrate:OPTical:LOADcommand.