:CALibrate:OPTical:STATus:REASon?
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Command Syntax
:CALibrate:OPTical:STATus:REASon
Query Syntax
:CALibrate:OPTical:STATus:REASon?
Description
Returns a string that explains the information on the status of the optical calibration. If the measurement was successful, the creation date for the file is returned. For example,
"Created: 01/19/2024 15:16:49"
If the calibration failed, the returned string would be something like "Missing module".
Use the :CALibrate:OPTical:STATus? query to determine if the measurement has failed.