:CALibrate:OPTical:MATTenuation
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations
Command Syntax
:CALibrate:OPTical:MATTenuation <max-allowable-attenuation>
Query Syntax
:CALibrate:OPTical:MATTenuation?
Description
During an optical path calibration, sets the maximum allowable attenuation (dB) above which the calibration fails. This setting can range from a minimum value of 3.0 dB to a maximum value is 30.0 dB. This setting can be set independently for each Fixture Lane calibration.
As of FlexOTO revision A.07.60, if during a calibration step a measured attenuation is above the maximum allowed, you can no longer force the calibration to accept the value by sending the :CALibrate:OPTical:UCURrent command. This command has been removed.