:CALibrate:OPTical:STARt
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations
Command Syntax
:CALibrate:OPTical:STARt
Description
Starts a calibration of all optical Hardware Diagram paths. For the optical calibration:
- Every optical path shown in the Hardware Diagram is calibrated.
- The nominal attenuation of a Demultiplexer's lanes or of an Impairement can be specified (not removed by calibration and so included in relevant measurements). Use these commands to enter the attenuaton:
- An optical source must be used.
- Use an optical power meter or DCA-X oscilloscope to measure the average optical power of the optical source. The average optical power must be between 100 μW and 2.000 mW. Enter the measured value using the
:CALibrate:OPTical:OPOWercommand before you start the calibration. - Connect the optical source to the first port on Fixture 1.
Follow this command with the query to control program timing.:CALibrate:OPTical:SDONe?
Example Script
The following Python code example is a very simple script just to demonstrate the very basic steps. It assumes a Hardware Diagram with one 2-lane DUT Fixture and one 2-lane WDM DUT Fixture. So, it must calibrate four lanes. For each lane, the script enters the average power of the optical source in line 8. In a real program, you would read the average power from your power meter or DCA-X and enter the unique average power level for each lane.
Copy
optical-calibration.py
import pyvisa as visa
rm = visa.ResourceManager(r'C:\WINDOWS\system32\visa64.dll')
FlexOTO = rm.open_resource('TCPIP0::localhost::hislip0,4880::INSTR')
FlexOTO.timeout = 20000 # Set connection timeout to 20s
FlexOTO.read_termination = '\n'
FlexOTO.write_termination = '\n'
FlexOTO.write(':CALibrate:OPTical:STARt')
FlexOTO.write(':CALibrate:OPTical:MATTenuation ' + '29.4')
while True:
message = FlexOTO.query(':CALibrate:OPTical:SDONe?')
message = message.replace('. ','.\n')
if 'Calibration has completed' in message:
break
step = FlexOTO.query(':CALibrate:OPTical:STEP?')
print('Step ' + step + '. ' + message)
power = input('\t\tEnter average optical power in mW ("2.0e-3" maximum): ')
FlexOTO.write(':CALibrate:OPTical:OPOWer ' + power)
FlexOTO.write(':CALibrate:OPTical:CONTinue')
filename = FlexOTO.query(':CALibrate:OPTical:LOAD:FNAMe?')
print('\n' + message + '\n\t\t' + filename + '\n\n')
FlexOTO.write(':CALibrate:OPTical:CONTinue')
pwrloss = FlexOTO.query(':CALibrate:OPTical:PLOSs?')
pwrlosslst = list(pwrloss.split(';'))
for path in pwrlosslst:
print('Measured path power loss: ' + path)
FlexOTO.write(':SYSTem:GTLocal')
FlexOTO.close()
The output of this script for my setup is shown here.
Step 1. "Connect an optical source to Port 1.1 (DUT Fixture 1 Lane 1) and specify the average optical power." Enter average optical power (eg, 4.0e-4): 380e-6 Step 2. "Connect an optical source to Port 1.2 (DUT Fixture 1 Lane 2) and specify the average optical power." Enter average optical power (eg, 4.0e-4): 400e-6 Step 3. "Connect an optical source with the appropriate wavelength to Port 1.5 (WDM DUT Fixture 2 Lane 1) and specify the average optical power below" Enter average optical power (eg, 4.0e-4): 4.2e-4 Step 4. "Connect an optical source with the appropriate wavelength to Port 1.5 (WDM DUT Fixture 2 Lane 2) and specify the average optical power below" Enter average optical power (eg, 4.0e-4): 3.9e-4 Message "Optical Calibration has completed successfully. The optical calibration data will be saved to the following file:" "C:\Users\kentb\Documents\Keysight\FlexOTO\Optical Calibrations\OpticalCalibration_2022-05-19_5.ocdx"