:CALibrate:OPTical:OPOWer
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Command Syntax
:CALibrate:OPTical:OPOWer <optical-input-power>
Query Syntax
:CALibrate:OPTical:OPOWer?
Description
An optical source is used to inject a signal of known power into each lane as they are calibrated. Use an optical power meter or DCA-X oscilloscope to measure the average optical power of the optical source. The average optical power must be between 100 μW and 5 mW.
Use this command to enter the average optical power measured for the current calibration of a Fixture Lane or accept the current value. As the optical calibration progresses, each lane of each optical path is calibrated.