:TPRogram:SLINe:EDIMage:FTYPe
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Command Syntax
:TPRogram:SETup:EDIMage:FTYPe {JPG | PNG | BITMap | TIFF | GIF}
Query Response
{JPG | PNG | BITM | TIFF | GIF}
Description
For a Station's selected Test Program line, selects the image file type when an eye diagram image is saved. To specify that an image be saved with the measurement results, add the EDIMage
argument to the :TPRogram:SLINe:MEASurements
command. The default setting is JPG
.
The command only applies to a selected line in the Test Program and is equivalent to the File Type field in the Selected Test Line Setup dialog. When adding new lines to a Test Program, use the :TPRogram:SETup:EDIMage:FTYPe
command.
Available Graphics Formats
The filename extension indicates the image file format. In SCPI commands and queries, the format is selected or indicated in a programming message by the strings shown in this table.
File Extension |
SCPI String |
Description |
---|---|---|
.bmp | BITMap
|
24-bit color symbol map file format. Bitmap, or .bmp, is typically used for storing symbol mapped graphic files. |
.png | PNG
|
Portable Network Graphics) format that is not compressed. It is widely accepted and is a good choice for both documents and the web pages. |
.jpg | JPG
|
24-bit color Joint Photographic Experts Group file format). .jpg is a graphics format that is compressed. This compression creates smaller files but may affect image quality. For example, data points may be erased due to the image compression. If file size is not an issue, use the .png format instead. The application uses the .jpg software written by the Independent JPEG Group. |
.gif | GIF
|
Graphics Interchange File format. .gif is a standard graphics format (256 color) used to store symbol mapped graphic files. For .gif files, this application uses LZW compression/decompression licensed under U.S. patent No 4,558,302 and foreign counterparts. The purchase or use of LZW graphics capability in a licensed product does not authorize or permit an end user to use any other product or perform any other method or activity involving use of LZW unless the end user is separately licensed in writing by Unisys. End user should not modify, copy, or distribute LZW compression/decompression capability. |
.tiff | TIFF
|
24-bit color Tag Image File format. .tif is a format of choice for storing images with lossless compression. It provides better quality, but larger files. This format is widely supported across platforms (PC, Mac, UNIX). This application uses LZW compression/decompression licensed under U.S. patent No 4,558,302 and foreign counterparts. The purchase or use of LZW graphics capability in a licensed product does not authorize or permit an end user to use any other product or perform any other method or activity involving use of LZW unless the end user is separately licensed in writing by Unisys. End user should not modify, copy, or distribute LZW compression/decompression capability. |