:JSOurce:AMPLitude

Flex Apps:
FlexPLL
Instrument:
M8000-Series
81160A

Command Syntax

:JSOurce:AMPLitude <amplitude>

Where <amplitude> is a double.

Query Syntax

:JSOurce:AMPLitude?

Description

Sets the amplitude (Vp-p single ended) on the FlexPLL source instrument's output signal. The default value is 400 mV.

When connecting the RF cable between the Source's output and the DUT's input, be aware that some PCI Express devices do not include an "on board" termination. In this case, if FlexPLL's default Source amplitude and offset settings are decreased, you may need to connect a 6 dB matching attenuator on the output of the Source.