:JSOurce:JPPeak

Flex Apps:
FlexPLL
Instrument:
M8000-Series
81160A

Command Syntax

:JSOurce:JPPeak <jitter amplitude>

Where <jitter amplitude> is a double.

Query Syntax

:JSOurce:JPPeak?

Description

Sets the jitter amplitude in seconds (sp-p) on the FlexPLL source instrument's output waveform. The default value is 50 ps.

Example Command

:JSOurce:JPPeak 5.0E-11