:JSOurce:PATTern
Flex Apps:
FlexPLL
Instrument:
M8000-Series
81160A
Command Syntax
:JSOurce:PATTern {PRBS7 | PRBS9 | PRBS11 | PRBS13 | SSPRq | CLOCk | CLOCk2 | CLOCk3}
Query Syntax
:JSOurce:PATTern?
Description
Selects a Pattern for the M8000-series Source's output signal. The Source's output waveform must be set to DATA rather than a CLOCk (:JSOurce:WTYPe command). In addition, use the :JSOurce:SCRate command to set the System Clock Rate, which automatically sets the Symbol Rate. Symbol Rate is the Source's output to your DUT.
The following table lists the arguments for the :JSOurce:PATTern command.
| Argument | Pattern |
|---|---|
PRBS7
|
27−1 pseudo-random symbol sequence (127 symbols). |
PRBS9
|
29−1 pseudo-random symbol sequence (511 symbols). |
PRBS11
|
211−1 pseudo-random symbol sequence (2,047 symbols). |
PRBS13
|
213−1 pseudo-random symbol sequence (8,191 symbols). |
SSPRq
|
Short Stress Pattern Random Quaternay PAM4 pattern (32,766 symbols). |
CLOCk
|
Selects a system clock rate. |
CLOCk2
|
Selects a system clock rate. |
CLOCk3
|
Selects a system clock rate. |
Example Command
:JSOurce:PATTern PRBS9