:JSOurce:COUPling
Flex Apps:
FlexPLL
Instrument:
M8000-Series
81160A
Command Syntax
:JSOurce:COUPling {AC | DC}
Query Syntax
:JSOurce:COUPling?
Description
Sets the output coupling for an M8000-series BERT Source's output channel to ac or dc. An 81150A or 81160A Source's output coupling cannot be changed. To select the M8000-series output channel, use the :JSOurce:CHANnel command.
Example Command
:JSOurce:COUPling DC