:JSOurce:CMODule
Flex Apps:
FlexPLL
Instrument:
M8000-Series
81160A
Command Syntax
:JSOurce:CMODule {MODule1 | MODule2}
Query Syntax
:JSOurce:CMODule?
Description
If the FlexPLL test setup includes an M8050A high-performance BERT as the jitter source, this command selects the location of the M8009A Clock Module in the AXEi chassis. The default value is MODule1.
Keysight recommends that you install the M8009A Clock Module in slot 1 of the AXIe chassis (or slot 2 if slot 1 is occupied by an embedded controller module) and the M8042A Pattern Generator in the next available slot.
Requires FlexPLL revision A.07.80 and above.
Example Command
:JSOurce:CMODule MODule1