:JSOurce:MODule:SNUMber?
Flex Apps:
FlexPLL
Instrument:
M8000-Series
81160A
Query Syntax
:JSOurce:MODule:SNUMber?
Description
Returns a serial number based on the type of source instrument:
- M8000 Series
- Returns the serial number of the physical BERT blade in the AXIe chassis. Use the
:JSOurce:SNUMber?query to return the BERT M8070 firmware serial number. - 81150A or 81160A
- Returns the serial number of the 81150A or 81160A function generator. For these instruments, the
:JSOurce:SNUMber?query returns the exact same model number.
To return the module number, use the :JSOurce:MNUMber? or :JSOurce:MODule:MNUMber?queries.