:JSOurce:MODule
Flex Apps:
FlexPLL
Instrument:
M8000-Series
81160A
Command Syntax
:JSOurce:MODule {MODule1 | MODule2}
Query Syntax
:JSOurce:MODule?
Description
Selects FlexPLL's connected M8000-series source instrument's BERT AXIe module. This command is only available if two or more BERT AXIe modules are installed in the M8000-series instrument. The default value is CHAN1. To enable or disable the output channel, use the:JSOurce:OENable command. This command does not work with an 81150A or 81160A source instrument.
Example Command
:JSOurce:MODule MODule2