:JSOurce:FORMat
Flex Apps:
FlexPLL
Instrument:
M8000-Series
81160A
Command Syntax
:JSOurce:FORMat {NRZ | PAM4}
Query Syntax
:JSOurce:FORMat?
Description
Specifies the type of modulation applied to the M8041A or M8045A BERT source's signal. Selections are NRZ (which is the default format) and PAM4. Note that the :JSOurce:WTYPe command must be set to select data output instead of a clock.
Requires FlexPLL revision A.06.80 and above.
Example Command Sequence
:JSOurce:WTYPe DATA :JSOurce:FORMat PAM4 :SYSTem:AUToscale *OPC?