:JSOurce:OENable
Flex Apps:
FlexPLL
Instrument:
M8000-Series
81160A
Command Syntax
:JSOurce:OENable {ON | OFF}
Query Syntax
:JSOurce:OENable?
Description
Turns on and off the FlexPLL source instrument's output channel. The default value state is OFF. To select the actual channel use the:JSOurce:CHANnel command.
Example Command
:JSOurce:OENable ON