:JSOurce:CHANnel
Flex Apps:
FlexPLL
Instrument:
M8000-Series
81160A
Command Syntax
:JSOurce:CHANnel CHANnelN
Where N is an integer that identifies a specific channel number.
Query Syntax
:JSOurce:CHANnel?
Description
Selects FlexPLL's connected source instrument's output channel. The default value is CHAN1. When the current channel is changed, FlexPLL automatically disables the channel to prevent against potential damage to an unterminated output. To turn the enable the channel, use the:JSOurce:OENable command.
Example Command
:JSOurce:CHANnel CHANnel2