:JSOurce:OFFSet
Flex Apps:
FlexPLL
Instrument:
M8000-Series
81160A
Command Syntax
:JSOurce:OFFSet <offset>
Where <offset> is a double.
Query Syntax
:JSOurce:OFFSet?
Description
Sets the signal offset in Volts on the FlexPLL source instrument. The default value is 200 mV.
When connecting the RF cable between the Source's output and the DUT's input, be aware that some PCI Express devices do not include an "on board" termination. In this case, if FlexPLL's default Source amplitude and offset settings are decreased, you may need to connect a 6 dB matching attenuator on the output of the Source.
Example Command
:JSOurce:OFFSet 2.0E-1