:JSOurce:WTYPe
Flex Apps:
FlexPLL
Instrument:
M8000-Series
81160A
Command Syntax
:JSOurce:WTYPe {CLOCk | DATA}
Query Syntax
:JSOurce:WTYPe?
Description
On M8041A, M8045A, or M8009A AXIe modules, specifies the output signal to be a clock or data signal. When the output signal is set to DATA, use the :JSOurce:FORMat command to select either NRZ or PAM4 data format.
An 81150A or 81160A source's output is always a clock and cannot be changed to data.
Example Command Sequence
:JSOurce:WTYPe DATA :JSOurce:FORMat PAM4 :SYSTem:AUToscale *OPC?