:RMEMory:COLor
Command Syntax
:RMEMory{1:4}:COLor TCOLor{1:16}
Where the {1:4} specifier identifies one of four possible JTF response memories. For example, :RMEMory3:COLor.
Query Syntax
:RMEMory{1:4}:COLor?
Description
Selects the color used to identify the selected response Memory plots on the JTF Graph. The selected color is applied to all three response Memory plots: JTF, OJTF, and JTF model. For example, if you select blue, the JTF plot is display as blue dots, the OJTF plot is displayed as a blue dotted line, and the JTF model is displayed as a solid blue line.
Waveform color assignments are saved as part of an instrument Setup file (:DISK:SETup:SAVe). Waveform colors are reset to their default values by a default setup (:SYSTem:DEFault) or factory preset (:SYSTem:FACTory).
| Color | Argument | Color | Argument | Color | Argument | Color | Argument | |||
|---|---|---|---|---|---|---|---|---|---|---|
| TCOLor1 | TCOLor2 | TCOLor3 | TCOLor4 | |||||||
| TCOLor5 | TCOLor6 | TCOLor7 | TCOLor8 | |||||||
| TCOLor9 | TCOLor10 | TCOLor11 | TCOLor12 | |||||||
| TCOLor13 | TCOLor14 | TCOLor15 | TCOLor16 |
To change the color of any waveform, use the following additional subsystem :COLor commands:
| Command | Description |
|---|---|
:RESPonse:COLor
|
Sets color of math function output waveforms. |
:RMEMory:COLor
|
Sets color of T-domain parameter or S-parameter waveforms in TDR/TDT mode. |
Requires FlexDCA revision A.04.50 for colors 13 through 16.
Example Command
:RMEMory2:COLor TCOLor5