:RMEMory:PLLModel:MEASure:DISPlay

Flex Apps:
FlexPLL

Command Syntax

:RMEMory{1:4}:PLLModel:MEASure:DISPlay {ON | OFF}

Where the {1:4} specifier identifies one of four possible JTF response memories. For example, :RMEMory3:PLLModel:MEASure:DISPlay.

Query Syntax

:RMEMory{1:4}:PLLModel:MEASure:DISPlay?

Query Response

{1 | 0}

Description

Turns the display of the Response Memory's model measurements in the results table on or off. If the :RMEMory:DISPlay parent command is set to OFF, this command will not be able to display the measurements.

Model Measurement's Effect on Measurements Displayed
Measurement :RMEMory:PLLModel:MEAS:DISPlay
Command
OFF ON
Maximum 1 ■ ■
Minimum 1 ■ ■
Average 1 ■ ■
Bandwidth ■ ■
Peaking ■ ■
Gain Frequency ■
Zero Frequency ■
Pole Frequency ■
Footnotes:
1. Displayed if :RMEMory:FLATness:MEASure:DISPlay command ON.

Example Command

:RMEMory2:PLLModel:MEASure:DISPlay ON