:RMEMory:PLLModel:MLOop:FGAin
Flex Apps:
FlexPLL
Command Syntax
:RMEMory{1:4}:PLLModel:MLOop:FGAin <loop gain>
<loop gain> is a double.
Where the {1:4} specifier identifies one of four possible JTF response memories. For example, :RMEMory3:PLLModel:MLOop:FGAin.
Query Syntax
:RMEMory{1:4}:PLLModel:MLOop:FGAin?
Description
Sets the frequency for the PLL loop gain for manually calculating the Response Memory JTF and OJTF model plots. Loop gain is the frequency at which the model JTF and OJTF curves intersect. The default value is 3.00 MHz, the minimum value is 1 Hz, and the maximum value is 1.00 THz.
Use the :RMEMory:PLLModel:ALOop:ENABle command to allow manual configuration of the JFT and OJTF models.
with Zero, Pole, and Gain Frequencies
Example Command
:RMEMory2:PLLModel:MLOop:FGAin 3.0E+6